MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
As your log refers to the C:/ path, it looks as though you are on a Windows computer. Is that correct, please? If you are using Windows then the link below has an illustrated guide for configuri...
-
That GitHub clone address is the correct one. If you continue to have problems, you can go to the GitHub repository page. https://github.com/IntelRealSense/librealsense Then click on the green ...
-
Hi Sh Sh Some D555 users have reported that the LEDs do not light even when the camera is operating normally, so this is not necessarily an indication of a problem. Please ensure that the USB ca...
-
Hi MUSTAFA CAYCI That guide is very old. I recommend using the excellent Lightbuzz guide at the link below, which can be used with both the old Intel-based Macs and modern Apple Silicon M machine...
-
Hi Yixun Liu Thanks very much for your questions. 1. It is fine to use non-RealSense post-processing filters. I would recommend using the RealSense ones for the filtering functions that are su...
-
Hi Aran Osinalde Can you first check the camera privacy settings in Windows please to ensure that permission for applications to access the camera is set to On. Instructions for doing so are in t...
-
It's great to hear that you were successful. Thanks very much for the update!
-
As it is an infrared type stream even though the image output is RGB, please use the Infrared 1 intrinsics.
-
Hi Yixun Liu Thanks very much for your questions. 1. When depth to color alignment is performed, the depth field of view resizes to match the color field of view size. If the color FOV is smal...
-
Ideally a streaming program using a RealSense camera will be closed down 'properly' by stopping the camera stream before exiting the program. Stopping streaming suddenly by closing the streaming p...