RealSense Support

My D555 camera is working

Comments

5 comments

  • MartyX Grover

    Hi Sh Sh  Some D555 users have reported that the LEDs do not light even when the camera is operating normally, so this is not necessarily an indication of a problem.

     

    Please ensure that the USB cable is not connected to the camera when using PoE as having USB plugged in will prevent the camera from working on PoE.

     

    In regard to testing the camera with USB, it should be detectable if you do not have the PoE ethernet cable plugged into the camera.  Are you using Windows or Linux, please?

    0
    Comment actions Permalink
  • Sh Sh

    I tried the camera only + usb with windows and i have tried to use linux windows and try to type ros2 topic list but the camera was not showing. Also I have tried to connect the camera through ethernet switch but it did not work when i tried to do ros2 topic list on Linux system in windows.

    0
    Comment actions Permalink
  • MartyX Grover

    Please use the instructions at the link below to confirm that the Windows camera privacy settings are set to On to allow access to the camera on a USB connection.

    https://github.com/IntelRealSense/librealsense/issues/3381#issuecomment-503424789

     

    The link below has an illustrated guide for configuring the D555's PoE ethernet settings in Windows.

    https://github.com/IntelRealSense/librealsense/issues/14293#issuecomment-3304919513

     

    0
    Comment actions Permalink
  • Sh Sh

    I confirmed Windows camera privacy settings are set to On but still same issue

    0
    Comment actions Permalink
  • MartyX Grover

    Which version of the RealSense SDK / RealSense Viewer are you using, please?  The oldest version that supports D555 is 2.56.4

     

    If your version is 2.56.4 or newer (the current latest is 2.57.4), the SDK needs to have been built from source code with CMake with the flag -DBUILD_WITH_DDS=ON included in order for the SDK to be installed with PoE support enabled.  The link below provides instructions about building the SDK on Windows from source.

    https://github.com/IntelRealSense/librealsense/blob/master/doc/installation_windows.md

     

    You can also build the SDK on Linux with CMake with the -DBUILD_WITH_DDS=ON flag included in the CMake build command.

     

    The USB cable chosen for use with the camera should be a high quality one suited for data transfer and not one that is only intended for charging up devices.

    0
    Comment actions Permalink

Please sign in to leave a comment.