RealSense Support

Post-processing of the depth map of human head using D405

Comments

1 comment

  • MartyX Grover

    Hi Yixun Liu  Thanks very much for your questions.

     

    1.  It is fine to use non-RealSense post-processing filters.  I would recommend using the RealSense ones for the filtering functions that are supported and the non-RealSense filters for the functions that the SDK does not support.

     

    2.  The filters are only applied to the depth image.

     

    3.  The parameters of the Temporal Filter are 'Filter Smooth Alpha' and 'Filter Smooth Delta'.  You can set them with code but you should not need to change these settings from their default values unless you have a depth image whose depth values are strongly fluctuating.

    0
    Comment actions Permalink

Please sign in to leave a comment.