MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi mml lmlm Raspberry Pi works best when built from source code on Ubuntu using the libuvc backend installation method at the link below. It it is also a very good method for use with non-Ubuntu ...
-
Hi Martin Studer Which of the two boards in the D435 camera did you replace, please? A D435 camera should have a D430 depth module board and a Vision Processor D4 V1 board. If it was the Visio...
-
Hi Rishabh Verma I have responded to your question at the issue below. Thanks! https://github.com/realsenseai/librealsense/issues/14588
-
Hi IACTICONTROL CTIcontrol It is not usually necessary to purchase a heatsink for the depth module and D4 V4 board. If the modules are in the open air then there is nothing to block the heat from...
-
Hi RERCA GMI GROUP If you purchased from the official RealSense Store then you can track your order using a link that can be found here: https://www.realsenseai.com/support/ If you would like to...
-
On the V5, a small physical switch needs to be moved sidewards with a small thin object like a pin, needle or paperclip to put it into USB mode, as by default it is set to use the GMSL connector. ...
-
Hi Raafe Asad Configuration guidance for Linux and Windows is provided at the links below. LINUX https://github.com/realsenseai/librealsense/issues/14284#issuecomment-3349204762 WINDOWS https://gi...
-
The Invalid SKU Error is only a risk when purchasing the V3 board and D450 separately. The 8-pack is the only way to be certain that this issue will not occur on V3. The SKU error would not occu...
-
Hi Terri Terri There are not many RealSense users using JP7 and Thor yet. In a recent case with a Thor user at the link below, I recommended running a new version of the L4T kernel patch script f...
-
If you are using a D450 depth module then a camera made with V3 or V5 will perform very similarly in terms of the image capabilities, including accuracy. Higher data transfer speeds will be possi...