RealSense Support

Realsense D555 PoE Connectivity Issues

Comments

1 comment

  • MartyX Grover

    Hi Raafe Asad  Configuration guidance for Linux and Windows is provided at the links below.

    LINUX

    https://github.com/realsenseai/librealsense/issues/14284#issuecomment-3349204762

    WINDOWS

    https://github.com/realsenseai/librealsense/issues/14293#issuecomment-3304919513

     

    Looking through your configuration details above, some other key details to bear in mind are:

    -  When using Linux, set the MTU value to 9000.  On Windows, it should be set to 9014

    -  The switch that you are using must support Jumbo Frames so that an MTU higher than the common switch default value of 1500 can be set.

    -  The subnet mask should be set to 255.255.255.0

    - The ethernet cabling needs to be CAT6 or higher, not the older CAT5.

    - The camera's ethernet cable should be plugged into the Out port on the switch.  The cable between the computer and switch should be plugged into the In port.

    -  If you have a USB cable attached to the camera, make sure it is disconnected before using the camera in PoE mode or PoE will not work.

    0
    Comment actions Permalink

Please sign in to leave a comment.