MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
1. Is this depth-only multi-second stall expected or known when using the D455 in Inter Cam Sync Mode 2? No. 2. Are there known D455 firmware issues involving the right-imager MIPI path or t...
-
Hi joosung lee D457 has a minimum depth sensing distance of around 50 cm, so it is appropriate for use at 50 to 60 cm range, though a It is a general physics principle (not specific to RealSense...
-
Hi Alexey Fokin Do you require further assistance with this case, please? Thanks!
-
Hi Hugh Feehan Do you require further assistance with this case, please? Thanks!
-
You are very welcome! 2. Yes, connecting the D450 depth module and Vision Processor D4 V3 forms a D455. The firmware driver identifies the model name by checking for what component parts are pr...
-
1. I can provide an example image of the heatsink, sandwiched between the depth module and Vision Processor D4, though information about its measurements is not available. The image is from the...
-
Hi Marian Fonseca Logs are unlikely to be useful for this particular issue, unfortunately. My past experience of this repeated disconnect-reconnect on Windows is that it may be related to a part...
-
RealSense do not sell the heat sink component separately or have a recommended supplier for it. The guidelines for choosing one yourself are straightforward though. It should ideally be slightly ...
-
Hi Ryan Lee Yes, combining a D450 depth module and Vision Processor D4 V3 forms a D455 with IMU, and the assembled camera is detected as D455 and has equal performance. In the cased D455 cameras...
-
Hi Charlie Barber Do you require further assistance with this case, please? Thanks!