RealSense Support

D455 Error Logs Not Appearing

Comments

2 comments

  • MartyX Grover

    Hi Marian Fonseca  Logs are unlikely to be useful for this particular issue, unfortunately.

     

    My past experience of this repeated disconnect-reconnect on Windows is that it may be related to a particular computer rather than the cameras, as it may occur on one PC but not another.  

     

    If you only have one camera at a time attached, and try each of the four cameras on their own individually, do you always get a successful and stable connection?  If you do then it could indicate that the computer is not providing sufficient power for the other cameras when multiple cams are attached and activated (the amount of power they draw from the computer increases when they are enabled).

     

    A way to test for the possibility of insufficient power is to use a mains electricity powered USB hub, which has more stable power than a hub powered by the computer as it draws the power for its USB ports from the mains plug socket instead of the computer's power supply.

    0
    Comment actions Permalink
  • MartyX Grover

    Hi Marian Fonseca  Do you require further assistance with this case, please?  Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.