MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
There is an Insert Image icon on top of the comment writing box to select and insert an image file, or you can copy a section of an image in a paint package with a selection tool and paste it direc...
-
Thank you very much. Could you provide more information about the statement As a starting point, I transform the camera origin to the world coordinate system please? The rs2_transform_pixel_to_po...
-
Hi Torsten Wilhelm Typically when using rs2_deproject_pixel_to_point with both depth and RGB streams enabled, depth-color alignment is first performed with the SDK's align_to instruction and then ...
-
As the problem is with the Dynamic Calibration tool, it does not sound like an issue related to the RealSense SDK version. The firmware version 5.12.13.50 that you have installed in the camera is ...
-
Hi Ahoffman This issue with re-generating blue areas in the Dynamic Calibration tool has been reported a couple of times recently. In both cases the problem was solved by using a procedure in the...
-
18181247 If there is a subject that you feel that you cannot discuss on this public forum due to issues of confidentiality, please email me at the address below. martyx.grover@intel.com ********...
-
1. As the Disparity Shift value is increased, the minimum depth distance of the camera decreases but the maximum observable depth distance of the camera also reduces. Whilst a Disparity Shift val...
-
Hi Henry, my understanding is that the smaller baseline of the D405 is part of what allows the image to remain in focus down to 7 cm without blurring. The larger baseline of the D430 could cause t...
-
The bottom of page 106 and top of page 107 of the data sheet have further guidance about cover material selection, citing uncoated clear acrylic (plexiglass) as an example of a cover material. Re...
-
It should not matter which SDK or firmware driver version is used with the camera on Windows 10. If your customer wants a configuration that they can feel assured about though then they could use ...