RealSense Support

Do D435 driver and firmware support Windows 10 21H2?

Comments

4 comments

  • MartyX Grover

    Hi Shigeyoshi Ohara  Yes, RealSense 400 Series cameras such as the D435 model cameras are compatible with Windows 10 21H2. I have 21H2 (also known as build 19044) on my main RealSense work computer, shown in the image below.  It is also on my personal PC that I successfully use RealSense cameras with.

     

    0
    Comment actions Permalink
  • Shigeyoshi Ohara

    Hello MartyG,

    Thank you so much for your quick answer. May I ask if you would know from which F/W and driver version support Win10 21H2? They just don't care Windows version?

     

    Regards,

    Ohara

    0
    Comment actions Permalink
  • MartyX Grover

    It should not matter which SDK or firmware driver version is used with the camera on Windows 10.  If your customer wants a configuration that they can feel assured about though then they could use Intel's recommended production camera configuration (one that can be used reliably with critical applications and commercial products that incorporate RealSense).  

    Intel's current recommended Production configuration at the time of writing this is SDK 2.50.0 and firmware driver 5.13.0.50

    https://dev.intelrealsense.com/docs/recommended-production-camera-configurations

    0
    Comment actions Permalink
  • Shigeyoshi Ohara

    Hi MartyG,

    I appreciate your support. I will recommend the customer to use the latest recommended configuration.

    Regards,

    Ohara

    0
    Comment actions Permalink

Please sign in to leave a comment.