MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Steve Steve Accuracy can be affected by a range of factors that do not just include distance from the camera. - Environmental lighting levels - The texture of the surface being observed by t...
-
Hi Kyle Coble The D555 camera model has its own separate datasheet that can be obtained from the link below. https://dev.realsenseai.com/docs/intel-realsense-d400-series-product-family-datasheet ...
-
Based on that link, I located the declaration of conformity with RoHS for the D435. https://www.intel.com/content/www/us/en/content-details/746827/camera-peripherals-intel-realsense-depth-camera-d4...
-
I located an Intel document from 2021 affirming the RealSense D455 camera's conformity with the European RoHS (Restriction of Hazardous Substances) regulation. The RoHS restricted substance list i...
-
Hi YinBin Ng All available regulatory certifications for RealSense cameras are available at the link below. https://realsenseai.com/regulatory-information/ If a particular certification is not l...
-
The intrinsics will change if you change the resolution from 1280x720 to another.
-
Hi IACTICONTROL CTIcontrol Changing the height, position or rotation of the camera should not affect these parameters. The position and rotation described in the extrinsics relates to the fixe...
-
Hi seongho ham Having the emitter enabled can enhance depth image quality, as it casts an invisible pattern of infrared dots onto surfaces in the scene that aids the camera's ability to analyze th...
-
Hi Eric, sincere apologies for the inconvenience. Whilst a D555 CAD file is not available at the time of writing this, as D555 uses the existing D450 camera circuit board you may be able to use th...
-
Aside from static interference, long cables should also be high quality ones, as performance degradation or camera connection drops are more likely to occur when using cables longer than 2 meters t...