RealSense Support

d435: <2% at 2 m

Comments

5 comments

  • MartyX Grover

    Hi Steve Steve  Accuracy can be affected by a range of factors that do not just include distance from the camera.

     

    - Environmental lighting levels

    -  The texture of the surface being observed by the camera (e.g how plain & smooth or detailed the surface is)

    -  Whether the surface is light colored or dark grey / black

    -   How reflective the surface is

     

    So whilst the official estimate of accuracy is <2% at 2 m, the actual accuracy in a real-world scene can vary depending upon the above factors. 

     

    RealSense cameras are calibrated in the factory during manufacture and are usually already well calibrated when received by the customer.  Cameras can become miscalibrated though if they experience a physical shock such as a hard knock, a drop on the ground or severe vibration, and performing a calibration can correct this.  So calibrating the cameras again before integrating them into your product is a good strategy.

    0
    Comment actions Permalink
  • Steve Steve

    What is the expectation of how far we should have to go with the calibration?
    Using the Chip and Tare...seem absolutely justifiable to me.

    But using the more intermediate method, or the OEM method certainly seem like more than should be required by a new product.

    And to note:  These are tested against your test image, 2m from the camera, in a well-lit environment.


    0
    Comment actions Permalink
  • MartyX Grover

    I have seen cases where a company has a team perform their own custom calibration of newly received stock of cameras before integrating it into their product.  So using On-Chip and Tare certainly is justifiable and normal for a commercial enterprise.

     

    On-Chip and Tare will be fine for most situations.  If a robust calibration is required then a commercial operation may opt to use the Dynamic Calibration tool instead.

    https://www.intel.com/content/www/us/en/download/645988/intel-realsense-d400-series-dynamic-calibration-tool.html

     

    The OEM tool is based on the Dynamic Calibration tool, with the added features of calibrating both intrinsics and extrinsics (the free public version at the above link only calibrates the extrinsics, though this is fine for the majority of users) and the ability to perform calibration remotely via a Linux server.  The OEM version, and the large-size OEM Calibration Target Board product for calibrating multiple cameras, are aimed at engineering departments and manufacturing facilities.

    https://store.realsenseai.com/buy-intel-realsense-d400-cameras-calibration-target.html

    0
    Comment actions Permalink
  • Steve Steve

    We're not doing a custom calibration; we are verifying the promised calibration before inclusion in the product.
    And simply trying to get that expected delivery.

    We have found the On-Chip and TARE to be helpful to get expected calibration numbers.
    But it's not foolproof.

    Trying to understand expected delivery quality.





    0
    Comment actions Permalink
  • MartyX Grover

    The official estimate of accuracy for the D435i model is <2% at 2 m so that should be your expectation, and RealSense cameras are usually already well-calibrated by default when received by the customer.

    https://realsenseai.com/compare-depth-cameras/

     

    The achieved accuracy during testing by the customer may be outside of that estimate but it will likely be due to factors in the testing environment having a negative impact on accuracy rather than a problem with the received hardware.

     

    What may work best for you is to reset the camera to its factory-new default calibration.  This will also resolve any miscalibrations that may have developed during transportation after the camera left the factory.  This can be done quickly in the RealSense Viewer tool using instructions here:

    https://github.com/IntelRealSense/librealsense/issues/10182#issuecomment-1019854487

     

    You could reset the calibration and then perform your verification afterwards so that you can be confident that the camera is as close to its expected <2% at 2 m accuracy as possible.

    0
    Comment actions Permalink

Please sign in to leave a comment.