RealSense Support

RealSense D457 emitter

Comments

1 comment

  • MartyX Grover

    Hi seongho ham  Having the emitter enabled can enhance depth image quality, as it casts an invisible pattern of infrared dots onto surfaces in the scene that aids the camera's ability to analyze those surfaces for depth information.  The dots will be less visible in brightly lit conditions though, so having the emitter enabled on a bright day may not have as great an effect as using the camera indoors under artificial lighting.

     

    The camera can though also use the ambient light in a scene to aid depth analysis.  The stronger the light, the better the camera can perform (however, reflective surfaces or directly facing the camera towards the sun can reduce depth quality). In summary, it's fine to leave the emitter enabled,  Whether the lighting conditions are bright or dim, the camera will be able to handle it.  By having the emitter enabled all the time, the camera will be able to cope with varying environmental conditions during the day and night.

     

    The strength of the emitter's projection reduces as distance from the camera increases.  You can increase the emitter's strength to its maximum to make the emission as visible to the camera as possible by maximizing the Laser Power setting to '360'.

     

    As the distance of an observed object or surface from the camera increases, accuracy reduces.  D455-type cameras such as D457 are capable of accurate long-range depth sensing.  Drift in accuracy should start to become noticeable beyond the 6 meter distance.  This is not because of the emitter strength though - it is a characteristic of the camera.  Error linearly increases over distance.  This phenomenon is called RMS Error.

    0
    Comment actions Permalink

Please sign in to leave a comment.