MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
If you have a USB cable, please test whether the camera is detectable on USB by disconnecting the ethernet cable and then connecting the USB cable and doing rs-enumerate-devices
-
If setting the IP to end in .70 does not work, the next step I would recommend trying is to enable dynamic camera IP discovery with DHCP using the command below so that the camera does not rely on ...
-
I note from the above information that your IPv4 address is set to 192.168.11.100. Please try setting 192.168.11.70 in the Windows network settings "Use the following IP address" if you have not d...
-
Hi Zirui Wang The recommended minimum firmware for D455F is 5.15.0.2 In regard to the output from the get parameter commands, they are what I would expect. - enable_infra1 and enable_infra2 are...
-
Is it detected if you run the rs-dds-config configuration program before rs-enumerate-devices ? rs-dds-configrs-enumerate-devices
-
Hi Sidket Criss Do you have a USB cable plugged into the D555 too? If you do then please disconnect it, otherwise the camera cannot operate in PoE ethernet mode. Have you tried changing the sub...
-
Hi Jeff Boucher The unfiltered stereo sensors of the D435 which are not equipped with IR-Cut filters can see all wavelengths in the visible to near-IR range, from around 400 nm visible up to aroun...
-
D455 has the same performance as D456 but without the dust / water resistant casing. So if the environment that the wood is being scanned in does not have dust / sawdust then D455 would be fine. ...
-
Hi Aakash Parmar If the camera will be positioned more than half a meter from the observed wood surface and will be operating in an industrial environment then the D456 RealSense model will likely...
-
Incomplete video frame detected is an extremely rare error. Does it occur if you plug one camera directly into the i9 computer's USB port? You could free up a port by unplugging the hub. If the...