RealSense Support

Unable to detect D555 PoE camera

Comments

11 comments

  • MartyX Grover

    Hi Sidket Criss  Do you have a USB cable plugged into the D555 too?  If you do then please disconnect it, otherwise the camera cannot operate in PoE ethernet mode.

     

    Have you tried changing the subnet mask to 255.255.255.0 in the Windows network settings as recommended in the illustrated setup guide for Windows?

    https://github.com/realsenseai/librealsense/issues/14293#issuecomment-3304919513

     

    On your PoE injector, is the ethernet cable between the computer and injector connected to the Data In port and the camera's ethernet cable connected to the Data Out port?

     

    Are you using a version of the SDK and Viewer that supports D555?  This would be version 2.56.4 or newer.

     

    Can you confirm please that you built the SDK on Windows from source code with CMake and included the flag -DBUILD_WITH_DDS=ON in the CMake build instruction?  This flag is necessary to enable PoE ethernet support in the SDK.  Instructions for a source code build can be found at the link below if you have not built the SDK from source on Windows already.

    https://github.com/realsenseai/librealsense/blob/master/doc/installation_windows.md

     

    Ignore the Enabling metadata on Windows instructions that come after the CMake installation instructions.

    0
    Comment actions Permalink
  • Sidket Criss

    Please find the following information of my configurations and steps perfomred.
    1. No USB cable connected. Camera is powered and connected only via PoE Ethernet.

    2. PC connected to LAN In
    3. Camera connected to Data + Power Out. The injector I use is TL-POE150S injector

    4. Built from source: Intel RealSense SDK 2.0 v2.57.6
    5. Built was successfull using following command.
    PS C:\librealsense\build> cmake .. -G "Visual Studio 17 2022" -A x64 -DBUILD_WITH_DDS=ON

    6. Detection results
    rs-enumerate-devices.exe
    No device detected

    rs-eth-config.exe --eth
    No RealSense devices found

    rs-dds-sniffer.exe
    listening on domain 0 (no output)

    C:\WINDOWS\system32>ping 192.168.11.55

    Ping statistics for 192.168.11.55:
        Packets: Sent = 4, Received = 4, Lost = 0 (0% loss),
    Approximate round trip times in milli-seconds:
        Minimum = 2ms, Maximum = 61ms, Average = 25ms

    7. Following is my network configuration
    Ethernet adapter Ethernet:

       Connection-specific DNS Suffix  . :
       IPv4 Address. . . . . . . . . . . : 192.168.11.100
       Subnet Mask . . . . . . . . . . . : 255.255.255.0
       Default Gateway . . . . . . . . . :
    8. Other info

    PC OS: Windows 10
    Ethernet adapter on PC: Intel I219-LM, link speed shows 1 Gbps
    Firewall: Disabled for testing
    Jumbo packet set to 9014 bytes


    Please guide me what's wrong, I been trying for days.

    0
    Comment actions Permalink
  • MartyX Grover

    Is it detected if you run the rs-dds-config configuration program before rs-enumerate-devices ?

     

    rs-dds-config
    rs-enumerate-devices
    0
    Comment actions Permalink
  • Sidket Criss

    I ran the commands you suggested. Please find the output I got.

    C:\librealsense\build\Release>rs-dds-config
    rs-dds-config 2.57.6.0

    -F- No device found supporting Eth
    -F- Did not apply requested configuration changes

    C:\librealsense\build\Release>rs-enumerate-devices
    No device detected. Is it plugged in?
    0
    Comment actions Permalink
  • MartyX Grover

    I note from the above information that your IPv4 address is set to 192.168.11.100.  Please try setting 192.168.11.70 in the Windows network settings "Use the following IP address" if you have not done so already.

     

    0
    Comment actions Permalink
  • MartyX Grover

    If setting the IP to end in .70 does not work, the next step I would recommend trying is to enable dynamic camera IP discovery with DHCP using the command below so that the camera does not rely on using its fixed IP address to be found.

    rs-dds-config --dhcp on
    0
    Comment actions Permalink
  • Sidket Criss

    Hi, please see results.

    Ethernet adapter Ethernet:

       Connection-specific DNS Suffix  . :
       IPv4 Address. . . . . . . . . . . : 192.168.11.70
       Subnet Mask . . . . . . . . . . . : 255.255.255.0
       Default Gateway . . . . . . . . . :

    C:\librealsense\build\Release>ping 192.168.11.55

    Pinging 192.168.11.55 with 32 bytes of data:
    Reply from 192.168.11.55: bytes=32 time=2ms TTL=64
    Reply from 192.168.11.55: bytes=32 time=2ms TTL=64
    Reply from 192.168.11.55: bytes=32 time=2ms TTL=64
    Reply from 192.168.11.55: bytes=32 time=3ms TTL=64

    Ping statistics for 192.168.11.55:
        Packets: Sent = 4, Received = 4, Lost = 0 (0% loss),
    Approximate round trip times in milli-seconds:
        Minimum = 2ms, Maximum = 3ms, Average = 2ms

    C:\librealsense\build\Release>rs-dds-config --dhcp on
    rs-dds-config 2.57.6.0

    -F- No device found supporting Eth
    -F- Did not apply requested configuration changes
    0
    Comment actions Permalink
  • Sidket Criss

    Same results with subnet mask 255.255.0.0 as you have shown in the picture.

    0
    Comment actions Permalink
  • MartyX Grover

    If you have a USB cable, please test whether the camera is detectable on USB by disconnecting the ethernet cable and then connecting the USB cable and doing rs-enumerate-devices

    0
    Comment actions Permalink
  • Sidket Criss

    I disconnected the Ethernet cable and connected camera with USB Cable, and tried the enumerate devices command, following is the output.

    C:\librealsense\build\Release>rs-enumerate-devices 
    No device detected. Is it plugged in?

    Also in device manager I see invalid descriptors.

    0
    Comment actions Permalink
  • MartyX Grover

    D555 is 'plug and play' in USB mode, meaning that it should be detected immediately upon insertion of the USB cable in the computer's USB port without having to make any special settings.

     

    If the camera cannot be detected even in USB mode then it indicates that the camera may be unfortunately dead.  In that case, I recommend contacting the retailer that you purchased it from to enquire about a replacement under warranty.

     

    If it was purchased from the official RealSense Store then you can use the web contact form at the link below, setting the topic as Return/Warranty.

    https://www.realsenseai.com/realsense-e-commerce-store-inquiry/

    0
    Comment actions Permalink

Please sign in to leave a comment.