RealSense Support

D455f driver

Comments

1 comment

  • MartyX Grover

    Hi Zirui Wang   The recommended minimum firmware for D455F is 5.15.0.2

     

    In regard to the output from the get parameter commands, they are what I would expect.

    - enable_infra1 and enable_infra2 are both disabled (false) by default, so have to be enabled in order to return as true.

    - enable_gyro and enable_accel are also disabled by default and so will return as false until they are enabled.

    0
    Comment actions Permalink

Please sign in to leave a comment.