MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Pgranitzka There are a range of options for extending the range of RealSense in a stable way. - High grade / industrial grade USB cables: cables longer than 2 meters are liable to experience ...
-
Hi Lghasemz The F200 and SR300 use a pattern projection method called coded light, also known as structured light, and are not stereo like the 400 Series cameras are. The technology is similar to...
-
Hi Chemicalx001 T265 related questions are handled on the RealSense GitHub forum. You can re-post your question there by visiting the link below and clicking the New Issue button. https://github...
-
Hi Diegobujanos The blue tone tends to be introduced into the RGB image if the White Balance setting has a low value. Increasing the White Balance causes the color in the image to normalise and t...
-
The best source of documentation for the RealSense ROS wrapper is its main page. Please scroll down through its various sections. https://github.com/IntelRealSense/realsense-ros You can also ask ...
-
Hi Rony The Jetson boards can experience problems with RealSense when multiple cameras are used on the same board. For single camera projects though, RealSense can usually work with the NX. Libre...
-
You do not need to build librealsense from the master branch on Windows. You can install it quickly and easily by downloading and running an installer file on the RealSense SDK Releases page. If y...
-
I tracked down the link to the case that I was thinking of about the inaccuracy in x and y when moving away from the center of the image. https://support.intelrealsense.com/hc/en-us/community/posts...
-
Are you asking please if accuracy of the depth measurements in an image may reduce as the coordinates move from the center of the image towards the sides of the image? If so then yes, this can hap...
-
Apologies for the delay in responding, as the question took some time to research. I located a past case that I handled where a RealSense user carried out the same kind of camera inclination test ...