Alessio Stella
- Total activity 23
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 9
Posts
Recent activity by Alessio Stella-
What's the point in using an external HW trigger or a SW trigger for L515?
Dear all I checked the interesting previous posts L515 inconsistent frame counts with external trigger – Intel RealSense Help Center L515 external hardware sync information – Intel RealSense Help ...
-
D455 with strobed light
Dear all is it feasible to apply a white strobed light in sync with the D455 and how? The purpouse would be to acquire a better RGB image As the D455 has a global shutter, i need the info of when t...
-
D415 RGB and IR spots pattern illumination cross talk. White Strobed/Pulsed illumination/lighting?
Dear all I noticed in an application a slight cross talk between RGB image and IR spot pattern illumination. I mean that in the RGB image i see many small coloured spots (mainly blue). Is that by c...
-
L515 complete asset
Dear all I have to buy a L515 for the first time and I wonder (1) is there one single model or are there different kinds of devices L515? I suppose the model is only one. (2) which optional/additio...
-
Using two D415 on the same FOV
Dear all I was wondering how to improve the accuracy of the depth given by a D415 and these are the three options i was thinking: 1. try repeating the automatic calibration 2. take more than one sc...
-
L515 global depth and image scan time - global latency, hence error between different pixels for a moving object
Dear all I am studying an application where I would have to scan objects of variable size moving at speed of 500mm/sec (about 20 inches/sec) on a belt scanned from above with a L515. Please conside...
-
L515 vs D415
Dear all could you please enlighten me on the main pros and cons of L515 vs. D415 and viceversa in industrial applications? Which main differences of performance they have and when one is more suit...
-
Intel RealSense D415 max length of USB cable
I am sorry I don't understand the specs. I see in the data sheet 15 inches max len. of the cable but I know of applications where the sensor is used with much longer cables? What is the precise sit...
-
Recommended Industrial PCs for use with Intel RealSense D415 in computer vision robotics applications
I am looking for a recommended industrial PC to develop a prototype of computer vision system for industrial robotic applications using your Intel RealSense D415 and your SDK with C++ on Linux or W...