RealSense Support

How to capture realsense RGB+IRs raw images.

Comments

13 comments

  • MartyG

    Hi Saeid. In regard to obtaining unrectified left and right infrared, it may be easiest to use the Y16 format, as it is unrectified because it is used for camera calibration.  Y16 can use 1280x800 at 15 and 25 FPS, and the Depth stream should not be enabled when streaming Y16 infrared.

    The link below provides further information.

    https://support.intelrealsense.com/hc/en-us/community/posts/360049233974-Can-you-access-raw-synchronized-D435-output-

    The link below provides a Python script for retrieving left and right infrared images that you could adapt.

    https://github.com/IntelRealSense/librealsense/issues/3878#issuecomment-569550710

    Whilst this link discusses accessing raw RGB frames with Python and OpenCV:

    https://github.com/IntelRealSense/librealsense/issues/7275

    0
    Comment actions Permalink
  • Saeid

    Hi MartyG , Thanks for your reply. I tried the python script you pointed out and modified it as follows to capture Y16, 1280x800 at 15 FPS:

    import pyrealsense2 as rs

    cntx = rs.context()
    device = cntx.devices[0]
    serial_number = device.get_info(rs.camera_info.serial_number)
    config = rs.config()
    config.enable_device(serial_number)

    config.disable_stream(rs.stream.depth)
    config.enable_stream(rs.stream.infrared, 1, 1280,800, rs.format.y16, 15)
    config.enable_stream(rs.stream.infrared, 2, 1280,800, rs.format.y16, 15)

    pipeline = rs.pipeline()
    profile = pipeline.start(config)

    Which results in this error:

     profile = pipeline.start(config)
    RuntimeError: Couldn't resolve requests

    I tried it with FPS 25 too and it results in the same error but it works with the original script's settings.

     

    0
    Comment actions Permalink
  • MartyG

    Y16 infrared 1 and 2 can only be streamed if the depth stream is not enabled too.

    0
    Comment actions Permalink
  • Saeid

    How the depth stream should be disabled?

    config.disable_stream(rs.stream.depth)

    above was added to do that although with/without it results in the same error.

    0
    Comment actions Permalink
  • MartyG

    You just need to delete the config.disable_stream(rs.stream.depth) line.  When using a custom stream configuration (cfg), the default configuration of the camera is overridden and only the streams that you define in the enable_stream lines will be enabled.

     

    0
    Comment actions Permalink
  • Saeid

    I tried without the config.disable_stream(rs.stream.depth) too and it results in the same error:

     profile = pipeline.start(config)
    RuntimeError: Couldn't resolve requests
    0
    Comment actions Permalink
  • MartyG

    The script looks fine.  I assume that you have an import pyrealsense2 as rs instruction on the first line.

    Could you confirm whether your camera is on a USB 3 connection please?   You can do this by launching the RealSense Viewer program and looking at the number beside the camera name in the options side-panel.  If the number is '2.1' then it is a USB 2 connection, and if the number is '3.2' then it is a USB 3 connection, because that mode is not supported on USB 2

    I ask this because Infrared 2 (the right infrared channel) is not accessible on a USB 2 connection and requires USB 3.  If the camera is not in USB 3 mode then requesting Infrared 2 would cause a Couldn't resolve requests error.

    0
    Comment actions Permalink
  • Saeid

    Yes I have the import pyrealsense2 as rs. I am connecting the camera through USB 3.2; confirmed with RealSense Viewer.

    0
    Comment actions Permalink
  • MartyG

    It occurred to me to check in the Viewer the settings it recommended for D415 in Y16 mode.  For the D415, the supported resolutions were one of these two, at 15 or 25 FPS:

    960x540

    1920x1080

     

    0
    Comment actions Permalink
  • Saeid

    Thanks MartyG! This seems to be working now for IRs. What will be the proper format, resolution, and FPS for capturing raw RGB images?

    0
    Comment actions Permalink
  • MartyG

    Obtaining raw unrectified RGB frames would be more complicated.  The link below discusses converting RAW16 color frames to RGB8 using Python.

    https://github.com/IntelRealSense/librealsense/issues/7275

    Whilst a case in the link below took the alternative approach of using MATLAB.

    https://github.com/IntelRealSense/librealsense/issues/8716

    0
    Comment actions Permalink
  • Saeid

    For the capture part of it would it be adding the following line to the above script?

    config.enable_stream(rs.stream.color, 0, 1920, 1080, rs.format.yuyv, 15)

     

    0
    Comment actions Permalink
  • MartyG

    I suspect that obtaining YUYV with that method would result in a rectified image rather than a raw frame.

    Y16 is also available as an RGB format, although it is grayscale.  You can test this by changing YUYV to y16 in the above line of code.

    0
    Comment actions Permalink

Please sign in to leave a comment.