Steve Steve
- Total activity 57
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 2
- Subscriptions 18
Posts
Recent activity by Steve Steve-
d555 built on d455? --> Can't get the same Framerate/Resolution as the d455
I've got a d455 and a d555I would like to operate the PoE at 90FPS 848x840Like I do with the d555That appears to be impossible??The closest I get--through awkward manipulation of the Realsense View...
-
d555 POE Ideal Range
This feels like a dumb questionBut all other devices specify an "Ideal Range"The d555 indicates it's built on the 450 series.So is it's "Ideal Range" something like:0.6m to 6mThere must be a reason...
-
d435: <2% at 2 m
We recently received an order of a number of the d435i cameras.We have a small team that checks the devices for accuracy before inclusion in the product. Defined as: <2% at 2 m Which I interpret...
-
Suggestions on how to protect against static.
I’m looking for suggestions on how to protect the camera from static.While I wouldn’t call it common, it’s definitely not unusual for us to see cameras partially disconnect from Windows when static...
-
435 Error Over Time at 90fps
With a diagnostic tool running, I've allowed the 435 cameras to run overnight.At the 4hr mark, the errors were nominal.Over time, were seeing the Critical Frame Drops start to add up dramatically.(...
-
Should we update Firmware?
General question.We've been using the 435 for several years now,.We locked into FW v5.13.00.50 during development.(newer FW versions require adoption of a new SDK)Looking at newer updates in firmw...
-
435 USB 3.0 and Static
Noticing, especially this time of year, a lot of static related issues.We use these cameras exclusively with Windows PCs.In high static environments, the Cameras disconnect from the PCs.They won't ...
-
435 Calibration Stability
When we receive a shipment of cameras, we test their calibration to make sure they are within our operating spec.If necessary, we do a quick calibration on them...I've seen some returns lately, and...
-
Adding Additional IR to the Scene, can it be helpful?
Our team has been sending out supplementary IR light since our product release.(It's never been explained well, and I've always considered it witchcraft. I've no evidence it's ever helped.) Today ...
-
FOV vs. Output Resolution
I'm trying to rectify something in my mind, I'm sure is simple.I'm not a programmer, I don't have experience with the SDKLooking at the 455 (depth) Field of View: 3:2 Output Resolution: 16:9 How...