RealSense Support

d555 built on d455? --> Can't get the same Framerate/Resolution as the d455

Comments

1 comment

  • MartyX Grover

    Hi Steve Steve  Page 3 of the version 1.1 data sheet document for the D555 camera describes that on a PoE connection the maximum FPS it supports is 60, and the streams support 896x504 instead of 848x480.

    https://realsenseai.com/wp-content/uploads/2025/08/D555-Datasheet-v1.1.pdf

     

     

    I do not currently have information regarding why 896x504 resolution is used instead of 848x480 on D555 PoE.

     

    Ethernet cables support a slower data transfer rate than USB 3 cables.  Ethernet cables have a maximum data transfer speed of 1 Gbps (gigabits per second), compared to 5 Gpbs on a USB 3 cable.

    0
    Comment actions Permalink

Please sign in to leave a comment.