Steve Steve

  • Total activity 57
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 2
  • Subscriptions 18

Activity overview

Latest activity by Steve Steve
  • Steve Steve created a post,

    d555 built on d455? --> Can't get the same Framerate/Resolution as the d455

    I've got a d455 and a d555I would like to operate the PoE at 90FPS 848x840Like I do with the d555That appears to be impossible??The closest I get--through awkward manipulation of the Realsense View...

  • Steve Steve created a post,

    d555 POE Ideal Range

    This feels like a dumb questionBut all other devices specify an "Ideal Range"The d555 indicates it's built on the 450 series.So is it's "Ideal Range" something like:0.6m to 6mThere must be a reason...

  • Steve Steve commented,

    MartyX GroverI was curious about temperature too.the datasheet defines the test as: "Ambient means environment while the camera is attached to a tripod using the cameras' tripod screw attachment a...

  • Steve Steve commented,

    We're not doing a custom calibration; we are verifying the promised calibration before inclusion in the product.And simply trying to get that expected delivery.We have found the On-Chip and TARE to...

  • Steve Steve commented,

    What is the expectation of how far we should have to go with the calibration?Using the Chip and Tare...seem absolutely justifiable to me.But using the more intermediate method, or the OEM method ce...

  • Steve Steve created a post,

    d435: <2% at 2 m

    We recently received an order of a number of the d435i cameras.We have a small team that checks the devices for accuracy before inclusion in the product. Defined as:  <2% at 2 m Which I interpret...

  • Steve Steve commented,

    We've continued to see issues.So, we've done a test with two cameras and the RealSense Viewer.We leave the viewer and cameras active.I don't see any issues after the first 24hrs.But by 72hrs...ther...

  • Steve Steve commented,

    Thanks for the specific cable recomend!  (Really...thanks!)I tested and rejected 3 cables from different manufacturers just yesterdayWe'll take a look at the code sample--thank you.I know we are al...

  • Steve Steve commented,

    Because the issue isn't uncommon...we've explored software solutions to allow us to reset the camera(s) Historically, power-cycling the cameras will resolve the issues encountered with static.  Bu...

  • Steve Steve commented,

    I've forwarded your cable suggestion to our team..thank you.We've found many of the long USB cables out there to be unreliable.We've been using an expensive flexible polymer optical cable from Mono...