Usef Desouky

  • Total activity 9
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Comments

Recent activity by Usef Desouky Recent activity Votes
  • I have replaced the ethernet connection with type-c but the camera is still not detected.I think the main problem is in the camera as I have connected d435 to the cable and it was detected successf...

  • Actually, we cannot determine the currently installed firmware version because the camera is not discoverable by the RealSense tools. However, DDS discovery still detects the camera participant (D5...

  • yes even the configuration as you see is correct, I cant ping the D555 at 192.168.11.55 and its not functioning properly

  • camera is not functioning well, please find the following setup  

  • no I cant reinstall ROS2 as its natively installed and this will delay the robot development.do you have a ready docker image for the d555 realsense with ros2?No I havent tried to use fastdds as cy...

  • My research of ROS_DOMAIN_ID=22 indicates that it is used to isolate nodes so that they will only communicate with other nodes, computers or robots that use ROS_DOMAIN_ID=22.  Is this what you are ...

  • But I need to change the camera domain id to match the ROS_DOMAIN_ID I have set not the oppositehere are some logs of the recent command so you can understand the problem top left: ping camera ip a...