Usef Desouky
- Total activity 9
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Usef Desouky-
Usef Desouky commented,
I have replaced the ethernet connection with type-c but the camera is still not detected.I think the main problem is in the camera as I have connected d435 to the cable and it was detected successf...
-
Usef Desouky commented,
Actually, we cannot determine the currently installed firmware version because the camera is not discoverable by the RealSense tools. However, DDS discovery still detects the camera participant (D5...
-
Usef Desouky commented,
yes even the configuration as you see is correct, I cant ping the D555 at 192.168.11.55 and its not functioning properly
-
Usef Desouky commented,
camera is not functioning well, please find the following setup
-
Usef Desouky commented,
no I cant reinstall ROS2 as its natively installed and this will delay the robot development.do you have a ready docker image for the d555 realsense with ros2?No I havent tried to use fastdds as cy...
-
Usef Desouky commented,
My research of ROS_DOMAIN_ID=22 indicates that it is used to isolate nodes so that they will only communicate with other nodes, computers or robots that use ROS_DOMAIN_ID=22. Is this what you are ...
-
Usef Desouky commented,
But I need to change the camera domain id to match the ROS_DOMAIN_ID I have set not the oppositehere are some logs of the recent command so you can understand the problem top left: ping camera ip a...
-
Usef Desouky created a post,
D555 PoE
Hi Realsense Support,I recently purchased the D555 camera, and overall it has been working quite well. Listing and echoing topics functioned smoothly for the most part; however, I encountered some ...