RealSense Support

D555 PoE

Comments

23 comments

  • MartyX Grover

    Hi Usef Desouky  If the problem started when you edited the ROS2 bashrc file, could you try resetting the file with the command below, which restores the file from a default template?

    cp /etc/skel/.bashrc ~
    0
    Comment actions Permalink
  • Usef Desouky

    But I need to change the camera domain id to match the ROS_DOMAIN_ID I have set not the opposite

    here are some logs of the recent command so you can understand the problem 



    top left: ping camera ip and cant detect camera over ethernet

    bottom left: rs-dds-sniffer on domain id 22 as the dds domain id in .realsense-config.json  set to 22

    top right: rs-dds-sniffer on domain id 0

    bottom right: locally exported ROS_DOMAIN_ID to 0 and on ros2 topic list I got the topics listed

     

    The issue that the camera is not discoverable and I need to get the topics listed on the ROS_DOMAIN_ID 22

    0
    Comment actions Permalink
  • MartyX Grover

    My research of ROS_DOMAIN_ID=22 indicates that it is used to isolate nodes so that they will only communicate with other nodes, computers or robots that use ROS_DOMAIN_ID=22.  Is this what you are attempting to do with your configuration, please?

     

    Is the RealSense DDS topic list detectable if you manually set the ID to 22 before you list the topics instead of relying on the automated definition in the bashrc file?

     

    export ROS_DOMAIN_ID=22
    ros2 topic list

     

    My research indicates that RealSense topics should be listable when the domain is set to 22.  However, those successes were in cases where the RealSense ROS2 wrapper had been installed and its node launched with the rs_launch.py launch file before echoing the topics.  For example:

     

    export ROS_DOMAIN_ID=22

    ros2 launch realsense2_camera rs_launch.py

    ros2 topic list

     

    My understanding is that when echoing the short list of RealSense DDS topics, a RealSense node is not yet active until the RealSense ROS2 wrapper has been launched by the user with rs_launch.py.  The short RealSense DDS topic list is able to be published without the RealSense ROS2 wrapper being launched because D555 is interoperable with Fast DDS, the middleware powering ROS 2.

    0
    Comment actions Permalink
  • Usef Desouky
    My research of ROS_DOMAIN_ID=22 indicates that it is used to isolate nodes so that they will only communicate with other nodes, computers or robots that use ROS_DOMAIN_ID=22.  Is this what you are attempting to do with your configuration, please?

    yes this is what I am attempting as the whole robot system runs on the ROS_DOMAIN_ID 22 and I want the camera topics to be discoverable across the system.

    Is the RealSense DDS topic list detectable if you manually set the ID to 22 before you list the topics instead of relying on the automated definition in the bashrc file?

    Unfortunately, no

    I tried launching with ROS_DOMAIN_ID 0 and ROS_DOMAIN_ID 22 but both had the same result

    ~$ ros2 launch realsense2_camera rs_launch.py 
    [INFO] [launch]: All log files can be found below /home/husarion/.ros/log/2026-06-03-15-29-16-907939-husarion-18475
    [INFO] [launch]: Default logging verbosity is set to INFO
    [INFO] [launch.user]: 🚀 Launching as Normal ROS Node
    [INFO] [realsense2_camera_node-1]: process started with pid [18478]
    [realsense2_camera_node-1] [INFO] [1780493357.319832862] [camera.camera]: RealSense ROS v4.57.7
    [realsense2_camera_node-1] [INFO] [1780493357.319947771] [camera.camera]: Built with LibRealSense v2.57.7
    [realsense2_camera_node-1] [INFO] [1780493357.319973196] [camera.camera]: Running with LibRealSense v2.57.7
    [realsense2_camera_node-1] [WARN] [1780493357.330568983] [camera.camera]: No RealSense devices were found!
    [realsense2_camera_node-1] [WARN] [1780493363.335267136] [camera.camera]: No RealSense devices were found


    I think we need to schedule meeting to solve this issue, kindly send me your contact details

    0
    Comment actions Permalink
  • MartyX Grover

    This RealSense support channel can only provide advice via web comments, unfortunately.

     

    Are you able to uninstall and reinstall ROS2 Jazzy to see whether the earlier configuration problems produced when the ROS_DOMAIN_ID was set in the bashrc file disappear?

     

    Have you previously tried accessing the topics with ROS2's default FastDDS to confirm whether or not the problem is related to use of cyclone_dds_rmw as you encountered some warnings?

    0
    Comment actions Permalink
  • Usef Desouky

    no I cant reinstall ROS2 as its natively installed and this will delay the robot development.
    do you have a ready docker image for the d555 realsense with ros2?

    No I havent tried to use fastdds as cyclone is recommended by the robot provider

    0
    Comment actions Permalink
  • MartyX Grover

    We do not have a ready-made official Docker image for ROS2.  Some RealSense ROS2 users have shared their Docker contents.  However, they are often designed for Nvidia Jetson, though the link below has one for PCs (amd64).

    https://github.com/2b-t/realsense-ros2-docker

    0
    Comment actions Permalink
  • Usef Desouky

    camera is not functioning well,

    please find the following setup

     

    0
    Comment actions Permalink
  • MartyX Grover

    Your D555 configuration settings appear to be correct.

     

    Some RealSense ROS users who switched to CycloneDDS have also increased the DDS buffer size to achieve improved performance.

    https://docs.ros.org/en/foxy/How-To-Guides/DDS-tuning.html#cyclone-dds-tuning

     

    https://github.com/realsenseai/librealsense/issues/14928#issuecomment-4249129238

     

    0
    Comment actions Permalink
  • Usef Desouky

    yes even the configuration as you see is correct, I cant ping the D555 at 192.168.11.55 and its not functioning properly

    0
    Comment actions Permalink
  • MartyX Grover

    Official support for ROS2 Jazzy and Ubuntu 24.04 in the ROS wrapper is included in the latest 2.58.2 beta SDK released yesterday.  So it may be worth trying that SDK to see whether your situation improves.

    https://github.com/realsenseai/librealsense/releases/tag/v2.58.2

     

    The Jazzy compatibility is provided via CycloneDDS, so it may be more compatible with your setup than previous SDK releases.

     

     The use of ROS_DOMAIN_ID=22 introduces uncertainty though, as this isolated domain is not usually used with RealSense cameras.

     

    As a next step, I would recommend installing 2.58.2 and then seeing if you are able to echo the short list of DDS native topics that do not require the wrapper by inputting ros2 topic list

    0
    Comment actions Permalink
  • mohamed mohamed

    We continued investigating the D555 PoE issue and have narrowed it down significantly.

    This does not appear to be a ROS 2 or ROS_DOMAIN_ID issue.

    Current Findings

    The camera is consistently detected as a DDS participant using rs-dds-sniffer:

    Participant 'D555_409122300110'
    

    We also observe DDS traffic directly from the camera IP (169.254.3.228) using tcpdump, confirming that the camera is powered, reachable over Ethernet, and actively transmitting DDS traffic.
    Regarding the SDK issue, we also tested with librealsense SDK v2.58.2 built from source. The behavior remained unchanged.

    However, the camera is still not discoverable by RealSense tools:

    • rs-enumerate-devices → No device detected

    • rs-eth-config → No RealSense devices found

    • RealSense Viewer → "Add Source (0 available)"

    The camera is visible on the network and DDS communication is active, but it cannot be discovered by any RealSense tools (rs-enumerate-devices, rs-eth-config, or RealSense Viewer).

    Could this indicate a hardware defect, or would you recommend additional diagnostics ?

    Attached 

    1. DDS participant discovery (rs-dds-sniffer)

    2. DDS traffic captured from camera IP using tcpdump

    3. RealSense Viewer showing "Add Source (0 available)"

    Thank you.

    0
    Comment actions Permalink
  • MartyX Grover

    Hi mohamed mohamed  When you built the SDK from source, can you confirm please if you included the CMake flag -DBUILD_WITH_DDS=ON in the CMake build instruction in order to enable DDS support in the SDK?

    0
    Comment actions Permalink
  • Wafaa Mohamed

    Thank you for the suggestion.

    Initially, I built librealsense v2.58.2 from source without explicitly enabling DDS support.

    After your recommendation, I rebuilt it with DDS enabled using:

    cmake .. \
      -DCMAKE_BUILD_TYPE=Release \
      -DBUILD_WITH_DDS=ON \
      -DBUILD_EXAMPLES=ON 
    

    I also tested another build with:

    -DFORCE_RSUSB_BACKEND=ON
    

    and another one without it.

    After rebuilding, the behavior remains unchanged:

    ./Release/rs-eth-config
    No RealSense devices found!
    
    ./Release/rs-enumerate-devices
    No device detected. Is it plugged in?
    

    However, DDS discovery is still working:

    ./Release/rs-dds-sniffer | grep D555
    Participant 'D555_409122300110'
    

    Additionally, I verified that the tools are using the newly built librealsense v2.58.2 library and not the system-installed version:

    ldd ./Release/rs-eth-config | grep realsense
    

    Output:

    librealsense2.so.2.58 => /home/husarion/librealsense_src/build/Release/librealsense2.so.2.58
    

     

    0
    Comment actions Permalink
  • MartyX Grover

    mohamed mohamed  Do you have a USB cable plugged into the camera?  If you do then it should be unplugged, as only the ethernet cable should be attached to the camera when using it in DDS mode.

     

    Is the camera connected to a 30 W PoE switch or 30 W PoE injector?

    0
    Comment actions Permalink
  • Wafaa Mohamed

    No USB cable is connected to the camera. The camera is operating in Ethernet DDS mode only.

    The camera is connected through a TSW101 PoE switch.

    DDS discovery is working and the camera appears as:

    Participant 'D555_409122300110'

    But rs-eth-config and rs-enumerate-devices still cannot detect the device.

    0
    Comment actions Permalink
  • MartyX Grover

    mohamed mohamed  Does the camera become discoverable if you enable DHCP dynamic discovery of the device with the command below?

    rs-dds-config --dhcp on
    0
    Comment actions Permalink
  • Wafaa Mohamed

    I tested the DHCP suggestion using both the locally built librealsense v2.58.2 tools and the system-installed tools, with the same result.

    rs-dds-config --dhcp on could not be applied because the camera is still not detected as an Ethernet RealSense device:

    -F- No device found supporting Eth
    

    However, DDS discovery still detects the camera successfully as:

    Participant 'D555_409122300110'
    

    So the D555 is visible on DDS, but it is not discoverable by the Ethernet configuration or device enumeration tools.

    0
    Comment actions Permalink
  • MartyX Grover

    Wafaa Mohamed  Do you know which D555 firmware driver version is currently installed in your camera, please?  The recommended firmware for SDK 2.58.2 is 7.58.38448.10612 which can be downloaded from the D555 Early Access firmware page.

    https://dev.realsenseai.com/docs/firmware-early-access-release-d500/

     

    Recent firmware versions, including this one, have improved camera discovery.

    0
    Comment actions Permalink
  • Usef Desouky

    Actually, we cannot determine the currently installed firmware version because the camera is not discoverable by the RealSense tools.

    However, DDS discovery still detects the camera participant (D555_409122300110).

    Is there an alternative method to retrieve the firmware version or update the firmware in this state? 

    Could this behavior indicate a firmware/configuration issue or a hardware defect? 

    0
    Comment actions Permalink
  • MartyX Grover

    If you have not been able to update the firmware since the camera was purchased then it likely still has the default factory-installed firmware on it, which is currently 7.56.19918.835, designed for use with SDK 2.56.4.

     

    It is recommended that D555 firmware updates are performed with a USB cable instead of the ethernet cable.  You mentioned earlier that no USB cable was connected to the camera.  Do you have a USB Type-C cable that you can attempt a firmware update with, please?

     

    If you have a USB cable then rs-fw-update and rs-enumerate-devices should also respond when the camera is on a USB connection.

     

    As the camera can be discovered in DDS mode to return D555_409122300110, it is likely that the camera hardware is okay.

     

    0
    Comment actions Permalink
  • Usef Desouky

    I have replaced the ethernet connection with type-c but the camera is still not detected.
    I think the main problem is in the camera as I have connected d435 to the cable and it was detected successfully.

    0
    Comment actions Permalink
  • MartyX Grover

    I note that the camera was working well when this support discussion began 23 days ago and then you begun experiencing problems with it after that.

     

    If you are using the camera on a USB cable with only USB plugged in and no ethernet cable attached, and the camera is still not being discovered by RealSense tools, then it does increase the chance that the camera has a fault.  If you purchased it recently then you have the option of contacting the retailer that you purchased it from to enquire about the possibility of an RMA return of the camera under warranty for a replacement.

     

    0
    Comment actions Permalink

Please sign in to leave a comment.