Tormod Slupphaug
- Total activity 19
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 6
- Subscriptions 4
Activity overview
Latest activity by Tormod Slupphaug-
Tormod Slupphaug created a post,
Extend usb cable 20 m
I need to extend the USB connection from my computer to a D415 camera to about 20 meters. I've looked at Newnex, but I'm a bit confused and overwhelmed by the plenty options. Cable length: the lon...
-
Tormod Slupphaug commented,
Q: "Are you asking please if accuracy of the depth measurements in an image may reduce as the coordinates move from the center of the image towards the sides of the image?" A: No, not really, tho...
-
Tormod Slupphaug commented,
Thank you for linking to some great articles Marty!From your reply, it seems I wasn't really clear enough when describing the issue. My apologies, I'll try to elaborate a bit, see comments below 😊 ...
-
Tormod Slupphaug commented,
MartyG: Got any input on this one? 😊
-
Tormod Slupphaug created a post,
Correlation between depth accuracy and accuracy of length measurements on surface/plane facing the camera
Hi, Depth accuracy of each of the Intel RealSense depth cameras can be found in the technical datasheets.However, I didn't find any documentation for accuracy/deviation when measuring distance betw...
-
Tormod Slupphaug commented,
I see. The D435 was chosen for its cheaper price and since it is also required to perform a reading of the pipe ID number (hard stamped on the pipe end). But the L515 also provides an RGB image? Wh...
-
Tormod Slupphaug commented,
Manufacturing facility with controlled lighting conditions. The lighting can be modified to achieve optimal results. Regarding the system described in the paper: If I'm not mistaken, I think it's...
-
Tormod Slupphaug commented,
Thanks MartyX Grover for the quick reply, I'll have a look at the paper. 😊 The camera and pipe will be mounted in fixed positions, but the distance from camera to pipes can vary (Z ≈ 0,5 to 1,5 met...
-
Tormod Slupphaug created a post,
Measuring dimensions of a pipe
I want to measure the dimensions of a pipe using the D435, but where to start? Has there been any similiar (open-source) projects, or are there any code snippets that I can use as a starting point?...