MartyX Grover

  • Total activity 2417
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 1 user
  • Votes 1
  • Subscriptions 745

Comments

Recent activity by MartyX Grover Recent activity Votes
  • Thanks very much Eriko Mogi and Shigeyoshi Ohara for your patience and for providing the further information.  It sounds as though KT01 is the computer that the camera does not work with, but it wo...

  • Hi Rohit  The tripod supplied with the D455 is useful for most of the positions that the IMU calibration tool requests, as you can rotate the tripod with your hand or pivot the camera on its mounti...

  • When you say "but one succeeds and the other fails", do you mean that you have tried the camera on two different computers that have antivirus software installed and the camera works on one of thes...

  • In the Android case in the link below where this error was occurring, the RealSense user in that case found that it was because the application was destroying the pipeline when restarting.  They fi...

  • Hi Handrian  The link below has a simple C# multiple camera example script for automatically creating a separate pipeline for each attached camera. https://github.com/IntelRealSense/librealsense/is...

  • The networking paper states that boards other than Pi can be used with the networking tool with minor modifications and cites Up Board as an example. https://up-shop.org/up-board-series.html I have...

  • Hi Joseslava  The Jetson Xavier could support multiple RealSense cameras.  For a 4-camera setup on a small computer form-factor though, you might like to also consider an Intel NUC mini PC with an ...

  • Is the camera detectable in the Windows Device Manager under its 'Cameras' category?     If it is detectable in the Device Manager, have you tried the camera with RealSense programs other than the...

  • I researched the problem carefully but could not find a way to alter the Uty wrapper to automatically flip an RGB image saved by the wrapper.  If it is a PNG image, you may have to flip the image m...

  • Having the camera plugged in during a Windows update should not affect the camera hardware (though Windows updates may introduce software issues that affect the camera's ability to operate in that ...