MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
There are few Python multiprocessing scripting references available other than the ones in the links below. https://github.com/IntelRealSense/librealsense/issues/7365 https://github.com/IntelRealSe...
-
Hi Lorenzo For a camera that can track fast motion (such as a moving arm / hand) for both depth measurement and RGB video and has a wide field of view, the RealSense D455 model would be an appropr...
-
Hi Yiming Liu If you click on the More option, is there an option in its menu to Update Firmware If there is, please follow the steps below. 1. Visit the firmware file archive at the link below...
-
Using pythagoras may be more complicated than is actually needed for this particular application. RealSense 400 Series cameras can be tilted (a maximum of 30 degrees would be best but beyond that ...
-
Hi Mustafatouqri236 As you are using pythagoras maths, may I first ask whether you are measuring the distance from the camera position to an object below the camera position (e.g at ground level),...
-
Hi Brice Miramont The RealSense discussion in the link below features a RealSense Python user who was importing multiprocess and using classes, and having problems with queues. It may provide som...
-
You are very welcome! The discussion in the link below about implementing hole-filling in Python will hopefully be of help to you. https://github.com/IntelRealSense/librealsense/issues/9899
-
On the camera with the worse depth image, please try enabling the Hole-Filling Filter in the Post-Processing Filter category if it is not enabled already in order to try to close the empty gaps. ...
-
If you increased Laser Power to maximum in the Viewer, did you increase it for each individual camera listed in the side panel under the Stereo Module options of each?
-
It looks as though the results are likely due to insufficient lighting in the location. The camera will have difficulty reading depth information from dark grey or black areas on the image. This ...