MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Thanks very much for the images. The far background and sides of the depth image look okay in terms of how the depth color-grading is shifting progressively from blue (near range) to red (far rang...
-
Hi Lukas Rauch - welcome to the RealSense community :) If you are new to developing C++ RealSense applications then the easiest way to integrate RealSense into your own project may be to use Windo...
-
Hi Lamlk1341 <2% is a good general value for describing the accuracy of a RealSense 400 Series camera. There are a range of factors though, such as environment and lighting, that can affect accur...
-
Hi Smeekim A measured distance of 1.5 m compared to 3 m real-world distance suggests that the camera may be mis-reading the depth due to some factor in the local environment, such as the location'...
-
Hi Jianfei Li Which RealSense SDK version are you using, please? If you are using firmware 5.12.12.100 then you should be using a minimum RealSense SDK version of 2.39.0. If your SDK version is ...
-
Hi Hploetz I performed a test call in Teams with a D415 and a D435i but didn't experience the problem that you described. You can perform a test call yourself in Teams by following the steps below...
-
Yes, I mentioned earlier in the discussion that the 1920x1080 PNG image seemed blurred, and the image import tool seems to agree, stating that Marks on plate are out of focus. When generating a PNG...
-
It's great to hear that you made significant progress! If the PYTHONPATH path variable has been defined correctly when building the pyrealsense2 wrapper then you should not need to place the two .s...
-
Halcon has dedicated software called HDevelop with functions in its Camera Calibration Assistant tool for calibrating with the calibration plate shown in your image. https://www.mvtec.com/products...
-
To check whether the blue area that is captured in the camera view at the higher resolution is responsible for the problem, I created a clean edit of the 1920x1080 image. Please right-click on the...