RealSense Support

gain performance get worse on color image after firmware update to 5.12.12

Comments

3 comments

  • MartyX Grover

    Hi Jianfei Li  Which RealSense SDK version are you using, please? 

    If you are using firmware 5.12.12.100 then you should be using a minimum RealSense SDK version of 2.39.0.  If your SDK version is earlier than 2.39.0 then I would recommend downgrading to firmware 5.12.7.100 as this was the last firmware before internal changes in the firmware introduced the need to use SDK 2.39.0 as a minimum when using firmwares newer than 5.12.7.100.

     

    If you are using the firmware in a commercial product then Intel recently categorized the currently latest 5.13.0.50 firmware as a Production (P) class firmware suitable for commercial applications.  The recommended SDK version for matching with this firmware is 2.50.0

     

    0
    Comment actions Permalink
  • Jianfei Li

    @MartyG I am glad to have your reply. we tried the minimum sdk still found it not desirable. we found that RGB images with firmware version 5.10.6 or earlier had an optimal internal gain, and it was more possible to obtain good images.

    which version of SDK is recommeded for firmware version 5.10.6?

    0
    Comment actions Permalink
  • MartyG

    5.10.6 was the recommended firmware for the RealSense SDK version 2.17.0 from November 2018. 

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.17.0

     

    0
    Comment actions Permalink

Please sign in to leave a comment.