MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Brice Miramont The main advantages of the OEM version of the Dynamic Calibration tool are to (1) calibrate both intrinsics and extrinsics, (2) calibrate remotely via a Linux server, and (3) be ...
-
The intrinsic parameters of the camera are described in the Intrinsics section of the SDK's Projection documentation in the link below. https://dev.intelrealsense.com/docs/projection-in-intel-reals...
-
Preset files are used by applications created in the RealSense SDK. Dot3D Pro is a software application that is compatible with RealSense camera hardware, not a RealSense SDK application. The co...
-
I note that your RGB exposure is set to 200 rather than 20 (the default RGB exposure value is 156). Or is the mention of 20 in your comment above a typo? :) If you are using manual exposure, yo...
-
If the dome is in an indoor location where the lighting level is consistent throughout the day, do you still see the effect if you disable auto-exposure so that the camera uses the default fixed ex...
-
It seems likely that pyrealsense2 is having difficulty with your Python installation, perhaps due to the mismatch between Python 3.9 and the pyrealsense2 files having been built for Python 3.8. If...
-
The error The ASIC temperature value is not valid is not necessarily an indication of a temperature problem. It can occur if the SDK is not able to provide a temperature reading at the moment that...
-
Whilst RealSense 400 Series cameras can work with any Intel or Arm processor, there is not such an assurance for AMD processors. In the small number of reported cases that have used computers with...
-
Ilya Nax If the SDK worked on the affected PC yesterday but not today, could you try installing SDK 2.50.0 again using the automated installer file in the 'Assets' list on the SDK Releases page. ...
-
Hi Kota Mogami A fix for helping to avoid frame drops was added to the SDK in 2.48.0. Here is the information from the release notes. Increase the syncer queue on model-views.h to avoid frame d...