MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
If there is a problem with a launch then it is worth trying initial_reset:=true first because it is easy to try, though it does not resolve every launch issue. The RGB color stream needs to be fu...
-
Thank you very much for the additional information. Your controller board has a very good hardware specification. If the camera is plugged into a USB 3,1 port but it is being detected as USB 2.0...
-
Hi tao wang It sounds as though you are using a single-board computer or controller board rather than a PC computer. Is that correct? If you are using a computing board / controller board, whic...
-
You are very welcome - thanks very much for the update!
-
Hi Ryan Lee Do you require further assistance with this case, please? Thanks!
-
Hi Harish Shelat Do you require further assistance with this case, please? Thanks!
-
The left and right sensors on D405 are IR sensors like the rest of the 400 Series family. D405 does not have a dedicated RGB sensor or an IR projector though. It does not have a projector because...
-
Hi Venkata Subbarao Thanks very much for your questions. 1. I have previously suggested using a visible dot pattern projector like the one at the link below, though I have not tested it myself....
-
Hi Harish Shelat The Lenovo Ideapad Miix700 12isk was released in 2016 and so the RealSense depth camera camera that is built-in is the R200 model. Typically, manufacturers who build RealSense in...
-
Yes, D401 can only use a USB Micro B cable for USB. You can purchase USB-C to USB Micro B adapters (please google for 'usb c to usb micro b adaptor' for more information), though as far as I am aw...