RealSense Support

Lenovo Miix700 12isk built in Camera not working in Windows10 or Ubuntu 26.04

Comments

2 comments

  • MartyX Grover

    Hi Harish Shelat  The Lenovo Ideapad Miix700 12isk was released in 2016 and so the RealSense depth camera camera that is built-in is the R200 model.  Typically, manufacturers who build RealSense into their products pre-install the camera drivers into the computer so that it is ready to use when the computer is bought.  This means though that if the computer is wiped to install another OS then the pre-installed camera drivers will be lost.

     

    The current generation of RealSense SDK software does not support the R200 camera.  In that era, R200 was intended to be used with Ubuntu 16.04 and did not have support created for later Ubuntu versions.

     

    The best option for R200 users is to install the original librealsense1 SDK, though it was not designed for OS versions newer than Ubuntu 16.04 or Windows 8.1.

    https://github.com/realsenseai/librealsense/tree/v1.12.1

    0
    Comment actions Permalink
  • MartyX Grover

    Hi Harish Shelat  Do you require further assistance with this case, please?  Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.