MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Thanks very much. I look forward to your next report. The link below has CUDA performance figures relating to align acceleration. https://github.com/IntelRealSense/librealsense/pull/2670
-
I only have one SR300 too unfortunately and no external IR illuminator and so cannot perform the test.
-
Which protobuf version did you use, please? The Acrobotic guide for Pi 4 and Raspberry Pi OS (formerly Raspbian) uses protobuf version 3.10.0. Some RealSense users found though that they had a sm...
-
You would still need to include an instruction to perform alignment. What CUDA support can do is significantly reduce the percentage usage of the CPU when performing alignment (it also accelerates...
-
Thanks very much for the tag correction, Lschreurs25 - I have adjusted the comment above! I note that you are using rs2::align. If you built the librealsense SDK on Jetson with CUDA support includ...
-
The control_transfer returned warnings in the log can be safely ignored if they are only appearing at the start of launch or appearing about once a minute instead of generating continuously. If th...
-
If you cannot find .so files, can you confirm please that your /librealsense/build/wrappers/python does not look like the Pi one below please? Also, can you describe the installation method that ...
-
1. The get_vertices() method is an accurate way of generating a pointcloud. It is possible that there are factors in the real-world scene that may be affecting accuracy. Would it be possible to ...
-
The age of the processor should not be a factor with 400 Series cameras, as they can work with any Intel or Arm processor. If the camera works fine on your brother's PC then it is likely that the c...
-
The link below has scripting for modifying the pointcloud.m example in the MATLAB wrapper to access a bag instead of live data. https://github.com/IntelRealSense/librealsense/issues/3241#issuecomme...