MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
The demo_pointcloud.launch file was created for the earlier ros2 branch (up to ROS2 wrapper version 3.2.3) and is not included in the new ros2_beta branch for the 4.x wrappers. I would suspect tha...
-
Hello, RealSense 400 Series cameras can interfere with infrared devices that are not 400 Series cameras, such as an SR300. The 400 Series camera should not experience interference in return from t...
-
If librealsense has been updated after the RealSense ROS wrapper has been built then the ROS wrapper needs to be built again. Did you perform a wrapper rebuild after installing the OpenMP-enabled ...
-
Hi Kota Mogami The firmware releases page states in its notes that 5.12.7.150 is the same as the 5.12.7.100 version that is listed. It is stated as the minimum firmware version for D435i and D455...
-
Which method did you use to install the RealSense SDK on your Windows computer, please? 1. With the automated installer file Intel.RealSense.SDK-WIN10 https://github.com/IntelRealSense/librealsen...
-
Hi Wildanazman072 Would the guide at the link below that uses RealSense, OpenVINO, OpenCV and ROS meet your needs, please? https://github.com/intel/ros_openvino_toolkit
-
The Stereo is NOT SUPPORTED message is likely a temporary glitch related to the processing struggles rather than a serious problem. Let's try generating a ROS2 pointcloud using a different launch...
-
I tested with the D405 but was not able to recreate your issue with seeing walls when testing with the RealSense Viewer at 15 cm range from the wall, even in dim lighting conditions. The camera us...
-
Is it able to detect a single camera in the Viewer if only one is plugged in? If it can detect one camera but not three in the Viewer, but it can list all three in the Device Manager, the problem ...
-
The Found 3 RealSense devices message that you highlighted is unusual if you only have one D455 attached, as the number of detected devices should reflect how many are attached. For example, in a ...