View my account

Unable to update D435i firmware

Comments

11 comments

  • MartyX Grover

    Hi Kota Mogami  The firmware releases page states in its notes that 5.12.7.150 is the same as the 5.12.7.100 version that is listed.  It is stated as the minimum firmware version for D435i and D455.

     

     

    The 30% stage on the progress bar is typically the point at which the RealSense Viewer's update mechanism performs a hardware reset of the camera before progressing to the next stage of installing the firmware.  So it sounds as though the camera is being reset and then the Viewer cannot re-detect the camera afterwards and time-outs.

     

    When attempting to update the firmware in the Viewer, are you doing so by selecting the Update Firmware menu option from the drop-down menu of the 'More' option and then selecting the Signed_Image_UVC_5_13_0_50.bin file that you downloaded to your computer, please?

     

    0
    Comment actions Permalink
  • Kota Mogami

    Thanks, MartyG.

    Oh, I understand about 5.12.7.150.

    Regarding the firmware update on realsense-viewer, yes, I select "Update Firmware" then selected the bin file "Signed_Image_UVC_5_13_0_50.bin" downloaded from the realsense firmware list page.

     

     

    0
    Comment actions Permalink
  • MartyX Grover

    Thanks very much for your patience.

    Let's check whether the camera can be updated in rs-fw-update when the tool is launched in recovery (-r) mode with the command below.

     

    rs-fw-update -r -f Signed_Image_UVC_5_13_0_50.bin

    0
    Comment actions Permalink
  • Kota Mogami

    Hi MartyG, 

    Hmm, recovery didn't work either.

    > rs-fw-update -r -f Signed_Image_UVC_5_13_0_50.bin 


    Update to FW: Signed_Image_UVC_5_13_0_50.bin

    No recovery devices were found!

    > rs-fw-update -l

    Connected devices:
    1) Name: Intel RealSense D435I, serial number: 141722078311, update serial number: 143523061992, firmware version: 05.12.07.150, USB type: 3.2
    0
    Comment actions Permalink
  • MartyX Grover

    Are you updating the firmware using the official short 1 meter cable that was supplied with the camera, please?  Using a longer cable of your own choice for a firmware update, especially 'active repeater' extension cables, is not recommendable.

     

    Do you have access to another computer that you can attempt the firmware update on?  The firmware is stored inside the camera hardware and not on the computer, so a firmware update made on one computer is carried over to another computer inside the camera.

    0
    Comment actions Permalink
  • Kota Mogami

    I actually don't have the official cable with me at this moment. However, I have tested this with several cables which work for other D435i devices. I also tested with several PCs both Windows and Ubuntu, but the update was never successful only on this D435i device.

    0
    Comment actions Permalink
  • MartyX Grover

    My research of your case only found a couple of previous cases of ERROR: Recovery device did not connect in time!  In one of them, the successful solution was to "restore Windows 10".  This could mean wiping and reinstalling Windows 10, but it could also mean using a Windows restore point (a save of an earlier Windows state) to roll back the computer to an earlier configuration where a problem was not occurring.  Restore points can only be saved if Windows already had the feature enabled in the past though.

     

    Next, let's try updating the firmware in an older version of the RealSense Viewer that still had an option called Install Recommended Firmware instead of the 'Check For Updates' option that the current Viewer has instead.

    Please visit the release page for the 2.44.0 version of the RealSense SDK at the link below and go to the 'Assets' file list.  Then left-click on the Intel.RealSense.Viewer.exe link to download it, and run the file to launch the 2.44.0 version of the Viewer after download has completed.

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.44.0

     

     

     

    Selecting 'Install Recommended Firmware' from the "More" menu should cause firmware 5.12.12.100 to automatically begin installing instead of needing to provide the firmware file (since the Recommended firmware was bundled in the Viewer).

    0
    Comment actions Permalink
  • Kota Mogami

    Hmm. I didn't try restoring Windows10, but testing realsense viewer of several versions including 2.44.0 didn't work.

    Anyway, thank you for your support, MartyG.

    0
    Comment actions Permalink
  • MartyX Grover

    Do you require further assistance with this case, please?  Thanks!

    0
    Comment actions Permalink
  • Kota Mogami

    That's fine at this moment. Thank you, MartyG.

    0
    Comment actions Permalink
  • MartyG

    You are very welcome.  Thanks very much for the update!

    0
    Comment actions Permalink

Please sign in to leave a comment.