MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
If the camera is pointing upwards then it is likely that there will be nothing in the camera's view except for a series of blobs that represent insects. In that case, an OpenCV tutorial in the lin...
-
Hi Farashes The ideal depth sensing range for the D455 model is stated by the data sheet document for the 400 Series cameras to be 0.4 meters to 6 meters. https://dev.intelrealsense.com/docs/int...
-
Hi Amelie Roy There is not yet an official CAD file for the D405. The D405 is though added to the new March 2022 edition of the data sheet document for the 400 Series cameras at the link below. h...
-
My research of your case only found a couple of previous cases of ERROR: Recovery device did not connect in time! In one of them, the successful solution was to "restore Windows 10". This could m...
-
Hi John Yang There is not an end of life (EOL) date planned for the 400 Series at the time of writing this, and the new RealSense D405 model that is suited to very close range accurate depth sensi...
-
Are you updating the firmware using the official short 1 meter cable that was supplied with the camera, please? Using a longer cable of your own choice for a firmware update, especially 'active re...
-
Hi Lojunkai98 As the D405 does not have a built-in projector, it cannot see in the dark without a light source present in the scene. The images below are taken in a room with no light, and when o...
-
Thanks very much for your patience. Let's check whether the camera can be updated in rs-fw-update when the tool is launched in recovery (-r) mode with the command below. rs-fw-update -r -f Signed...
-
RealSense cameras are calibrated in the factory and are well calibrated already when purchased. There are circumstances where a camera may become mis-calibrated and should undergo recalibration th...
-
It's great to hear that your problem is solved. Thanks very much for the update!