MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Ronghao Jonathantan May I begin by confirming what the shadowing effect that you are referring to is - the black outline around your body, or the rough black area at the bottom of the image? T...
-
Hi Charlie This issue regarding exposure drop to minimum is very rarely reported in the present day after fixes such as adding support for fractional exposure to the auto-exposure algorithm were i...
-
Hi Timothy P Baxter Social Vision Processor D4 board versions typically work with certain RealSense models. For example, the D450 depth camera board (the circuit board inside the D455) requires V...
-
Do you require further assistance with this case, please? Thanks!
-
The 20 m image shown earlier was separate Depth and Left IR images of detail observed at 20 m, with depth on the left and IR on the right. Distance does not restrict the range of the IR image, alt...
-
Hi Maharshi Oza The Vision Processor D4 chip does not allow customized code. The camera sensor components can be individually controlled directly though with the Low-Level API. https://dev.intelr...
-
The section of Intel's camera tuning guide linked to below provides a formula for calculating RMS error. https://dev.intelrealsense.com/docs/tuning-depth-cameras-for-best-performance#section-verify...
-
Hi Jane Haslam D401 is the camera circuit board inside the D405's casing. The D405 therefore cannot be used with external triggering. In the RealSense Viewer, the D405 does though support the a...
-
Hi Tschweh1 There have not been any reported problems with magnets during the history of RealSense products. The original RealSense R200 stereo depth camera model (the predecessor of the modern 4...
-
The link below provides Python resources for programming a depth Threshold Filter in the RealSense SDK to control the distance rendered on the depth image. https://github.com/IntelRealSense/libreal...