MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Shigeyoshi Ohara Yes, RealSense 400 Series cameras such as the D435 model cameras are compatible with Windows 10 21H2. I have 21H2 (also known as build 19044) on my main RealSense work computer...
-
I just wanted to highlight that the brew install librealsense method of installing librealsense on Mac now lists support for MacOS Monterey and for Apple Silicon M1. This method is also compatible...
-
Another RealSense-compatible option for people and moving-object tracking is Teleidoscope. Its entry on the RealSense software information page lists that it is Unity compatible. https://teleidosc...
-
If you will be using Raspberry Pi OS (formerly Raspbian) then yes, the same /video system as regular Linux should apply.
-
Hi Hoyeneyi Would it be possible to post a copy of your ROS launch log from the terminal in a comment below please, including the messages that are logged during runtime after launch has completed...
-
Hi Thomas Specte It is fine to place a custom housing with a transparent window around a cased RealSense camera that already has front glass. At the link below, a RealSense team member provides a...
-
Thank you, your firmware version looks fine. When you try to access the camera in a video application, can you confirm that the camera is not already being actively used in another application suc...
-
Hi Paul Pelluchon As RealSense 400 Series cameras are stereo depth technology, you can output left and right infrared simultaneously as a pair of monochrome images in Y8 or Y16 format. The white d...
-
The only supported FPS for 1280x720 is 6 if the D435i camera is on a USB 2 connection, where the supported resolution / FPS modes of the camera are limited. 1280x720 at 30 FPS is accessible when t...
-
Hi Yixun Liu The physical size and focus of RealSense imaging sensors are fixed.