MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Yixun Liu Typically in the RealSense Android wrapper, pause and resume commands take the form of onPause and onResume instructions, as demonstrated in the section of the Playback Android exampl...
-
Hi Makoto Terabayashi You cannot define an Advanced Mode parameter such as Second Peak Threshold (also known as Second Peak Delta) in a launch file directly. You could though define it in a json c...
-
The full range of RealSense flexible interposer cables (individual and multipack) are now in stock in the RealSense Store at the time of writing this. https://store.intelrealsense.com/
-
I ran extensive tests with the target image. I found that the detection was most likely to fail if the target was not absolutely centered in the yellow box right from the start of when the calibra...
-
You should not have to manually add a GT value when performing Tare calibration in the RealSense Viewer. Point the camera at the printed target and left-click on the Get button to generate your ow...
-
Hi again Adnan. The self-calibration white paper now has a PDF version of the 11x17" target for Tare and focal length calibration at the link below. https://dev.intelrealsense.com/docs/self-calibr...
-
Further information about Tare can be found in Intel's self calibration white-paper guide at the links below. https://dev.intelrealsense.com/docs/self-calibration-for-depth-cameras#31-running-the-t...
-
Hi Ron Vis There have only been a small number of RealSense support cases involving FPGA in the past. They have usually been about Xilinx Ultra96 FPGA (using Petalinux) or PYNQ-Z1 / PYNQ- Z2. X...
-
Hi Lucas Marti If your depth image is fluctuating then please first try lowering the Temporal Filter's Filter Smooth Alpha value from 0.4 to 0.1 to reduce fluctuation. I also note that the Post-Pr...
-
If an index number is not defined for the infrared stream when using only left infrared instead of both left and right then it should default to using the left stream.