MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Update: the D555 CAD file is now available at the link below under the Depth Cameras heading. https://dev.realsenseai.com/docs/stereo-depth-camera-d400#cad-files
-
Hi Marcin Adamek The D555 CAD file and full D555 datasheet are not yet available at the time of writing this. I check the CAD and datasheet pages regularly and have added this discussion to a lis...
-
Hi Steve Steve Depth measurement error starts at around zero at the front of the camera and increases linearly over distance as the distance between the camera and the observed object / surface in...
-
Hi Amit Bohra By default the D457 is set to use a GMSL cable instead of USB. To set the camera to operate on a USB connection you need to open a small removable cover on top of the camera and move...
-
Hi cam test I note that you mention that you are using the D457 'module'. Can you confirm please whether you are using a D457 camera, or a D450 depth module board and Vision Processor D4 V5 board...
-
On-Chip calibration relates to enhancement of depth quality. To enhance accuracy, the Tare calibration tool is used. Z-accuracy reduces and error increases as the distance from the camera of an ...
-
Hi Anukkah Burleson You are not doing anything wrong. The download link is broken. I will raise the issue with my RealSense colleagues. In the meantime, as an alternative to using calibration ...
-
Frame Metadata can be enabled on Windows in the RealSense Viewer tool. When the program is launched, there will usually be a pop-up box that appears in the top corner informing that metadata is di...
-
Hi Patrycja Grabowska Can you check the camera privacy settings in Windows please to ensure that permission for applications to access the camera is set to On. Instructions for doing so can be fo...
-
Hi Mercio Jonova There have been a couple of past cases where users of FLIR thermal imaging cameras have attempted to align them to the depth of RealSense cameras, so that may be a helpful referen...