RealSense Support

D455: Depth map is only acquired in a central cross shape, missing in the corners

Comments

6 comments

  • MartyX Grover

    Hi bomin kim  The missing areas on the depth image appear to correspond to darker, less strongly illuminated areas on the RGB image.  The camera may be having more difficulty with analyzing those areas for depth detail.

     

    In the Stereo Module > Controls section of the RealSense Viewer's options side-panel, please try maximizing the Laser Power option's value to '360' to increase the strength of the laser projection from the camera's projector component.  Does maximizing Laser Power reduce the size of the empty black areas on your depth image?

    0
    Comment actions Permalink
  • bomin kim

    No, adjusting the laser power did not resolve the issue. The same problem occurs when capturing different scenes. It seems like it's not related to lighting conditions or parameter values.

    0
    Comment actions Permalink
  • MartyX Grover

    If changing Laser Power does not make a difference, please next go to the Stereo Module > Post-Processing  section and expand open the list of post-processing filters.  Find one called 'Threshold Filter' which is enabled by default with a blue icon next to it and left-click on the blue icon to turn it red (off) so that the camera can depth-sense to its full range.

     

    If the depth remains missing, left-click on the red icon next to the Hole Filling filter to turn the icon blue (on) and cause the missing depth to be automatically filled in.

    0
    Comment actions Permalink
  • bomin kim

    I have already tried all of these steps.
    The problem still isn’t resolved.

    Could it be a calibration issue?

    0
    Comment actions Permalink
  • bomin kim

    Or could it be a hardware issue itself?

    0
    Comment actions Permalink
  • MartyX Grover

    You could eliminate mis-calibration as a cause by enabling the depth stream and then using the instructions at the link below to reset the camera to its factory-new default calibration in the Viewer, if you have not tried this already.

    https://github.com/IntelRealSense/librealsense/issues/10182#issuecomment-1019854487

    0
    Comment actions Permalink

Please sign in to leave a comment.