MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Thank you. And there is no difference if you change the stream index from -1 to 0 ?
-
In your Unity project, which version of the realsense2.dll file are you using, please? D455f support was introduced from SDK version 2.54.1 onwards. So you need to have a version of the DLL files...
-
Hi Sujeet Jha The D455f camera model will support 5 FPS as a minimum at 1280x720 resolution instead of the 6 FPS that D435 cameras support. If your camera is detected as being on a USB 2.1 speed...
-
Hi Dhyan Patel The two circuit boards inside the camera (the Vision Processor D4 and the D430 Depth Module) can be used without the casing. These boards can actually be purchased separately witho...
-
Hi chen guo Which method did you use to install the librealsense SDK, please? For computing devices based on the RK (Rockchip) chipset, building the SDK from source code with the libuvc backend i...
-
Hi Wout Oude Elferink Please email me your contact details (name, company name, website address, telephone number, etc) and I will pass them to the appropriate RealSense team member. You can cont...
-
If you ordered a V1 board then the camera will appear as D435. There is no way for it to become a D435i if a V1 board is used because the IMU hardware component is on the Vision Processor D4 board...
-
Some RealSense cameras and boards are out of stock worldwide at the moment, If you are located in South Korea as your name suggests then the best chance of fixing the camera quickly might be to or...
-
Hi Johannes Rabe The bottom of page 42 provides information about the infrared projector component's wavelength frequency (around 850 nm near-IR) and which IEC regulations it is compliant with. ht...
-
If the camera was purchased less than 12 months ago then it would have been under warranty, but opening the camera to inspect the RGB cable will have unfortunately voided the warranty so it cannot ...