RealSense Support

Change D455f frame size/resolution with Unity asset

Comments

9 comments

  • MartyX Grover

    Hi Sujeet Jha  The D455f camera model will support 5 FPS as a minimum at 1280x720 resolution instead of the 6 FPS that D435 cameras support.

     

    If your camera is detected as being on a USB 2.1 speed connection instead of the faster USB 3.2 then at 1280x720, the 30 FPS speed will be unavailable and only 5 FPS will be supported.

    0
    Comment actions Permalink
  • Sujeet Jha

    0
    Comment actions Permalink
  • Sujeet Jha

    even at 5fps also it's not working MartyX Grover

     

    0
    Comment actions Permalink
  • Sujeet Jha

    0
    Comment actions Permalink
  • MartyX Grover

    In your Unity project, which version of the realsense2.dll file are you using, please?  D455f support was introduced from SDK version 2.54.1 onwards.  So you need to have a version of the DLL files in the RealSense folder of your Unity project that is from version 2.54.1 or newer.

     

    The instructions at the link below describe how to obtain a recent version of the RealSense DLLs and import them into your Unity project.

    https://github.com/realsenseai/librealsense/discussions/11944#discussioncomment-6297523

    0
    Comment actions Permalink
  • MartyX Grover

    Thank you.  And there is no difference if you change the stream index from -1 to 0 ?

    0
    Comment actions Permalink
  • Sujeet Jha

    after changing script of RSDevice now it's working but the problem is that i'm not getting good accuracy. like on a flat surface it,s jittering a lot compare to 640*480, any suggestion?

    0
    Comment actions Permalink
  • MartyX Grover

    The link below provides advice about implementing post-processing filters in the Unity wrapper.

    https://github.com/realsenseai/librealsense/issues/1898

     

    If a Temporal filter is implemented then its 'Filter Smooth Alpha' setting can be used to reduce depth jittering.

    0
    Comment actions Permalink
  • MartyX Grover

    Once the camera starts streaming, a RealSense Device Inspector configuration interface should appear in the Unity side-panel.  So you could also try increasing the Laser Power setting during runtime from '150' to its maximum of '360' to see if it helps the camera to analyze the flat surface better by strengthening the pattern of invisible IR dots projected by the camera.

     

     

    Changing the Visual Preset from 'Custom' to 'Medium Density' may also help with accuracy.

    0
    Comment actions Permalink

Please sign in to leave a comment.