MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi Mderuijter Not all settings that are defined in the RealSense Viewer are exported to a custom json, which may be why certain options such as Histogram Equalization do not update if you load the...
-
Hi Waseemshariff126 If you are using Windows then rs-convert.exe should be in the Tools folder. This folder can be found by right-clicking on the RealSense Viewer launch shortcut icon that is pla...
-
RealSense 400 Series cameras are calibrated in the factory and so have very good calibration when they are new out of the box after purchase. You can perform a calibration of an individual camera ...
-
Hi Lghasemz I am well, thank you. :) As indicated by your kindly provided image, your camera is in Recovery Mode, suggesting that something went wrong during your firmware update such as the proc...
-
Hi Szalontai Martin As you are already using pointcloud.calculate, you could store the result of that operation in a numpy array and then print the coordinates from the array. The link below has ...
-
Hello, if you will be using the 5 cameras simultaneously then I would recommend selecting an industrial PC with an i7 CPU due to the processing demands of streaming that quantity of cameras at the ...
-
Hi Payaxig841 Although some camera models are being discontinued, the 400 Series stereo depth models (including the D455) are continuing. RealSense depth cameras are not dependent on a licence / ...
-
Hi Karthikeyan Yuvraj You can access the intrinsic and extrinsic information of a RealSense camera using the RealSense SDK's rs-enumerate-devices tool. Launching the tool with the instruction rs-...
-
Hi A Nunez Given the symptoms that you describe, I will refer your case to a team member of this Intel RealSense Customer Support forum. Thanks very much for your patience.
-
Hi Maharshi Oza If you are referring to the multi-colored line at the top of the depth image, variations on this phenomenon have been reported before in a few cases on Linux, but usually not on Wi...