MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
Hi JINGJING LIU Multiple RealSense 400 Series cameras do not interfere with each other and overlapping their fields of view can actually improve depth analysis. This is because each camera projec...
-
Hi Disha Rathod If a stream starts slowing down after a predictable amount of time has passed then I would first recommend checking whether the application has a memory leak, where available compu...
-
There was a past case of this start error reported in 2023. A solution was not found in that case, unfortunately. And the age of your firmware means that you will not be able to use the alternati...
-
Results could vary depending on the camera viewpoint, as RealSense cameras lacking filtering that are directly facing a strong light source can have their sensors saturated with light, causing prob...
-
The plain black areas on the depth image do correspond closely to the position of ceiling lights or areas where their light is being strongly cast onto reflective surfaces such as the horizontal gi...
-
Hi Ryan Lee What distance is the camera from the observed surface, please? It is recommended that a D455f is placed at least 60 cm away. This is because RealSense cameras have a minimum depth se...
-
Hi Joe Haynes Do you require further assistance with this case, please? Thanks!
-
Hi ChenLin Yeh Thanks very much for your questions. 1. Readout begins when exposure is completed. So the length of the exposure time should influence when readout starts. I do not have a spec...
-
Hi Richard Li Yes, < 0.25 health check score means that the calibration is very good. Ghost data is not an indication of a problem with the camera hardware and would not merit a return of the ca...
-
It's no trouble at all. I appreciate you letting me know about your success!