RealSense Support

Technical question about RealSense D455 camera-side latency for low-latency application

Comments

2 comments

  • MartyX Grover

    Hi ChenLin Yeh  Thanks very much for your questions.

     


    1.  Readout begins when exposure is completed.  So the length of the exposure time should influence when readout starts.  I do not have a specific value available for the latency at 848×480 @ 90 FPS though.

     

    2.  I agree that SENSOR_TIMESTAMP would likely be the best representation of the image exposure time as it marks the middle of sensor exposure.

     

    3.   FRAME_TIMESTAMP marks the beginning of UVC frame transmission (the first USB chunk sent towards the host).

     

    SENSOR_TIMESTAMP and FRAME_TIMESTAMP are both generated by the firmware driver and both use the same clock.  Their relation is that SENSOR_TIMESTAMP << FRAME_TIMESTAMP.  More information about how different types of timestamp behave can be found here:

    https://github.com/realsenseai/librealsense/issues/2188#issuecomment-409985803

     

    4. Your suggestion of FRAME_TIMESTAMP - SENSOR_TIMESTAMP seems valid. Though a D455 user at the link below who was exploring latency took the alternative approach of calculating latency with TIME_OF_ARRIVAL - FRAME_TIMESTAMP

    https://github.com/realsenseai/librealsense/issues/11667

     

    5.  The SDK's frame buffering documentation at the link below describes how "latency in the system will come from system level buffering done in drivers or software".  

    https://github.com/realsenseai/librealsense/wiki/Frame-Buffering-Management-in-RealSense-SDK-2.0#latency-vs-performance

     

    By default the frame pipeline can hold a maximum of 16 frames of each type of stream at a time, and the oldest frames get pushed out of the frame queue by newly arriving frames.  The pipeline is already configured by default for minimum latency.  Introducing latency into the queue can improve stability and reduce the number of dropped frames if more than one stream is being enabled.

     

    6.  For this question I recommend to you Section 4.5 (Latency) of RealSense's 'High-Speed Capture Mode' white-paper document, which provides detailed technical information about latency.

    https://dev.realsenseai.com/docs/high-speed-capture-mode-of-intel-realsense-depth-camera-d435/

     

    This section states that "the depth camera itself introduces very little latency because it has no full frame buffer, which means that images by necessity flow through the ASIC with ~100 lines of latency".

     

    7.  As mentioned in question 3, the FRAME_TIMESTAMP reflects the beginning of UVC frame transmission.

     

    8.  If the emitter is disabled then the IR image could become under-exposed unless the lighting in the scene is strong.  

     

    9.  The default settings of RealSense 400 Series cameras are configured for optimal performance and minimal latency.  So I would recommend using the default of auto-exposure being enabled.

     

    10.  rs-data-collect is an excellent tool for profiling low-level camera performance.

     

    To configure the infrared stream to 848×480 @ 90 fps, you should edit the stream width, height and FPS parameters in the rs-data-collect.h file of the project and then build the source code of the program so that it can use the updated parameters.
    https://github.com/realsenseai/librealsense/blob/master/tools/data-collect/rs-data-collect.h#L13

     

    The Low-Level API can produce the best possible latency, but there is not much documentation for it and the rs-data-collect program is the only example program I am aware of that demonstrates code for accessing this API.

    https://github.com/realsenseai/librealsense/blob/master/doc/api_arch.md#low-level-device-api

     

    You could also consider trying the rs-latency-tool example program.

    https://github.com/realsenseai/librealsense/tree/master/wrappers/opencv/latency-tool

    0
    Comment actions Permalink
  • MartyX Grover

    Hi ChenLin Yeh Do you require further assistance with this case, please?  Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.