MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
This RealSense support channel can only provide advice via web comments, unfortunately. Are you able to uninstall and reinstall ROS2 Jazzy to see whether the earlier configuration problems produc...
-
My research of ROS_DOMAIN_ID=22 indicates that it is used to isolate nodes so that they will only communicate with other nodes, computers or robots that use ROS_DOMAIN_ID=22. Is this what you are ...
-
Hi Usef Desouky If the problem started when you edited the ROS2 bashrc file, could you try resetting the file with the command below, which restores the file from a default template? cp /etc/skel/...
-
You are very welcome. Thanks very much for the update!
-
Hi Richard Li Do you require further assistance with this case, please? Thanks!
-
Hi Menghuan Yang Do you require further assistance with this case, please? Thanks!
-
In terms of RealSense cameras, the stereo baseline distance is the distance between the center-line of the left and right IR sensors. As the left and right sensors are mounted on the circuit board...
-
1. If a camera is mis-calibrated (if that is what you mean by out-of-calibration) then the depth image could have elements that should not be there and would likely not be there on a camera with a...
-
If you need to move the D405 closer than the default minimum depth distance of 7 cm in order to perform extremely close examination, a setting in the Viewer called Disparity Shift can be used to re...
-
Hi Menghuan Yang It is possible to measure volume in the RealSense Viewer tool using a bag file without programming your own solution. The steps for doing so are: 1. Open the Viewer without th...