MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
With C++ and Python there are two approaches that have been used as a workaround: - Put the sensors on separate pipelines (IMU on one pipeline and depth / color on the other pipeline); or - Use c...
-
The coefficients are deliberately all set to zero on the 400 Series cameras, so this is not an indication of a problem. https://github.com/IntelRealSense/librealsense/issues/1430 Calibration readi...
-
Yes, LibRS is shorthand for librealsense. You may also see it described as LRS, librealsense2 or RealSense SDK 2.0 in some places.. Whilst librealsense 2.31 is certainly usable, I would encourage ...
-
Hi Dserbes1 The RealSense 400 Series cameras can export data to file in a range of formats, such as rosbag (the most efficient recording method), PNG image, csv, (textual information), raw (an ima...
-
There may be no further corrective action that can be taken with this particular camera unit, unfortunately. ************* 残念ながら、この特定のカメラユニットで実行できる修正措置はこれ以上ない可能性があります。
-
I will refer it back to Intel again to take another look at it as a follow-up to my earlier discussion with them.
-
Hi Shibata664 1280x720 at 6 FPS is still available on D415 and D435 / D435i. If you are using a D455 then 5 FPS is available at 1280x720. The UWP driver 6.1.160.21 is not required for using RealS...
-
Hi Yzkzero The cameras are calibrated at the factory.
-
Could you try your D455 with the rs-capture sample program please? This should display depth, RGB and IMU stream panels in a single window. You can find a pre-made version of this program in Wind...
-
Ok, thank you very much. You should not downgrade the D455's firmware to match, as using a firmware in the D455 that is earlier than the most recent ones that introduced D455 support could break t...