MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
As well as setting the Master camera to '1' in the RealSense Viewer, have you also used the Add Source button to add the two Slave cameras to the Viewer too (so that you have three cameras listed i...
-
Hi Fabrizio Dini I should emphasise from the start that my pure C (not C++ or C#) knowledge is limited. I will do my best to provide some useful insights though. Yes, releasing resources is impor...
-
Hi Repele31 If you find it more comfortable to use a language other than English then please do and i shall do my best to help you in that language. Could you perform a full recalibration of your ...
-
Great news that the standalone Viewer was successful for you! Feedback reviews aren't required, but thanks for the thought - I'm pleased that I could be of help :)
-
Hi Simon Mcdonald Since SDK version 2.36, the version of the RealSense Viewer that is installed by the full Windows SDK installer has minimum requirements described in the link below. https://gith...
-
Sorry for the misunderstanding. You stated that the problem occurred whilst on a video call, so it sounded as though the camera was being used as a video conferencing webcam. :) This would be a...
-
If you are experiencing the RGB problem when using the camera in a video call application such as Skype, outside of SDK applications such as the RealSense Viewer, then it does suggest that the caus...
-
There are hand-eye calibration tools for robot arms that work with RealSense 400 Series cameras. Here are a couple of suggestions. autoCalibration https://github.com/IntelRealSense/librealsense/is...
-
Okay, thanks very much for the clarification. My reference above was based on a recent D435 case. So you have tried 1920x1080 Infrared and not found it to be of help, please?
-
Okay, thank you. The panels look like what I would expect for a D430i. I will seek input from another member of the RealSense support team. Thanks so much for your patience. @... Could you prov...