MartyX Grover
- Total activity 2417
- Last activity
- Member since
- Following 0 users
- Followed by 1 user
- Votes 1
- Subscriptions 745
Comments
Recent activity by MartyX Grover-
You are very welcome :) I cannot fnd a mention in this case of the librealsense version that you are using. However, there was a bug fix for valgrind in SDK 2.35.2 that is titled "Valgrind: Cond...
-
Hi M Faizan The discussions in the links below should be helpful in understadig the behavior of the IMU in the rs-motion example program. https://github.com/IntelRealSense/librealsense/issues/4391...
-
If you want to check whether there is an issue with your Pi 4 setup, you could install the Pi 4 SD card image of a librealsense installation provided by Intel in the link below. This can be helpfu...
-
Hi Najw111 Can you confirm please which presets you are referring to? If you are referring to Visual Presets, the SR300 / SR305 cameras have a different set of Visual Presets to the ones of the 400...
-
Hi Accounts Mmt I do not have any information on whether the minimum of 100 = no gamma correction at all, unfortunately. So I would not be confident in saying that it does. If you are seeking RGB...
-
Thanks for your patience whilst I performed further tests. A dynamic recalibration of the camera did not improve the apparent mis-scaling of the occlusion shadow around the hand. After extensive te...
-
A custom enclosure may have an effect on the image if the solid areas of the enclosure, such as the non-transparent border of the area where a transparent sensor window is placed, obstruct the sens...
-
Hi Jens Nirme I would recommend using the original cable supplied with the camera if you are satisfied with a 1 meter cable length. For longer cable lengths, cable quality is very important to avo...
-
If the Master is set to 1 and the Slaves to 2 and the slaves are not syncing their tinestamp, that would seem to point us back in the direction of a possible issue with the sending of the sync sign...
-
Hardware sync causes the timestamps of the Slave cameras to try to follow the timing of the Master camera. The slave cameras are still responsible for generating their own streams though - it does...